12/5/2018 9:13 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. I have a display that shows the position of a gear lever via a faceplate. The faceplate is a square that can be white, grey, green or red. The value is put into the faceplate via a DBW. I need to know which values correspond to which colors. I would like to to manually change the value of the DBW from 0 to 1 and then to 2 and all the way up to 255 and see which colors I get on the square. It is not possible to use the PLC for this investigation - I need to be able to simulate it with my WinCC engineering PC What is the easiest way to do this? I am thinking I can use the OS-simulation to see the square but how do I enter the increasing values? Attachmentsim.zip (75 Downloads) |
12/7/2018 7:24 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Is there really no one here that can give me some good advice on this matter? |
12/7/2018 6:05 PM | |
Joined: 9/21/2012 Last visit: 5/3/2024 Posts: 3937 Rating: (444) |
Start the HMI simulation with "Tag simulation" |
Follow us on