12/18/2018 3:11 AM | |
Joined: 10/20/2015 Last visit: 9/5/2023 Posts: 94 Rating: (19) |
Hello Frayer In the attachment a possible solution. This is extracted from an old program of mine. I currently don't have the time to test it because I am on the road for work. If it is not what you need or it doesn't work, please delete it AttachmentStep.zip (520 Downloads) |
12/18/2018 6:13 AM | |
Joined: 12/18/2014 Last visit: 5/3/2024 Posts: 32954 Rating: (4073)
|
Here from me a slightly different variant. A little clearer and requires fewer blocks. AttachmentSteps_0BA8.Standard.zip (529 Downloads) |
12/18/2018 6:39 AM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
Maybe Frayer is only asking for a power status display and the program to control Q1, Q2 and Q3 is ready. Then it is an easy way to create power display with two multiplexers and arithmetic block, see file in attachment. Regards, Scorp AttachmentStepdisplay.zip (506 Downloads) |
This contribution was helpful to1 thankful Users |
12/19/2018 12:07 AM | |
Joined: 12/3/2018 Last visit: 1/22/2024 Posts: 76 Rating: (0) |
Excuse me: what is this "VM mapping"? I never used Network inputs, can you explain purpose and use? I tried your program, but lower part for Power% doesn't work for me, did I enter something wrong? Since I don't know how to use Network inputs, I tried with normal inputs, but simulator gives me wrong number in %. Can you check program, did I do something wrong? AttachmentSteps_v2_by_ixo65.zip (487 Downloads) |
12/19/2018 6:39 AM | |
Joined: 12/18/2014 Last visit: 5/3/2024 Posts: 32954 Rating: (4073)
|
The VM area is a special memory area of the LOGO !, which is for data exchange between LOGO!s and/or LOGO! and remote devices. Tools> Parameter VM Mapping. AttachmentSteps_V2_0BA8.Standard.zip (513 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on