2/9/2009 9:06 AM | |
Posts: 54 Rating: (0) |
Hi all, I am Tuan, I need some helpfor running my CNC system. I have a 810DE (Export Version) with list divices below: 1) PCU50 2) OP12 3) Keyboard standard 4) MCP 483C 5) CCU 3.4 with CPU 314C-2DP (02 Axis FSD) 6) SIMODRIVE 611D Expansion powermodule with 02 Axis FSD. 7) 1PH Motor (01 pcs) 8) 1FT Motor (02 pcs) 9) HMI Advance V6.4 10) Tool box V6.5.2 for 810D/840D After install HW, install software, I download: a)HW configure to PLC with PLC315-2DP(I triedupload HW from PLC but it's have "?" symbol soItried tofind a HW for 810D with CCU 3.4 but have nothing in HW SINUMERIK Add-on, there isonly a 810D/840D HW including CCU 3 (Not CCU3.4) with PLC 315-2DP, it's warning that 810D/840D HW configure download to PLC is not appropriate PLC online when I startdownload but it't still running). b) Base program (In LibraryTABs on STEP7, with OB1 (Call FC2, FC19)OB40 (Call FC3), OB100 (CallFB1/DB7),...) After that, All devicesgoon MPI network, 187.5kbps, Addr: PCU:1, PLC:2, NCK:3, MCP:14. System is ready to runbut needs some settings for parameter. Ifollowed the Start-up guide to set parameter for system, but It could not run (In Jog mode example - I'm trying run dry Motor before doing anything more). System doesn't any error. Pls help me to know that: 1) With warning in HW configure but PLC isstill running,Is it a problem with system? 2) Which version of Toolboxdoes it have HW Add-on 810D with CCU 3.4 and where can I download it? 3) With all axisare FSD type, Cansystem run with 1PH Motor?How can I install it? 4) When I try to Jog in Start/Drives/servo/Auto. control setting: Press Start to run, is warning: Axis X1: Abort: Controller Enable missing. what does it mean? 5) When check some enable signals in Driver/servo/Servie data for each Axis, some signalsis NO: a) Pulse anable PLC b) Speed controller enable NC c) Ramp-func. gener. rapid stop d) Pulses enabled. when I check some signal in DB31 follow Start-up guide: DBB0: B#16#8 DBX1.3-1.7: false DBX2.1-2.2: false DBX4.3: false DBX4.6-4.7: false DBX5.0-5.5:false DBX20.1: false DBX21.7: false Pls tell me when willthey be"true"?We must set these bits or it will automatic come "true" with right configure? 6) This is the first time I configure and Start-up this system, it's so slowly and amateur, plsgive me some advises for better result? Hope to hear from you soonest. Nguyen Anh Tuan Automation Industrial Center Niem Tin Ltd. Co. - Hanoi - Vietnam. emails: tuan.nguyen-anh@ntc.com.vn or anhtuani3t@yahoo.com . website: www.ntc-vn.com |
2/11/2009 12:17 PM | |
Posts: 54 Rating: (0) |
Hi nulizhang, Great !!!! Thanks for your advises, I tried to do my system following your comment, It's okey, my system had running in Jog mode, I can use Jog +/- to turn 02servos motor: 1FT. But pls help me to know why the 1PH Motor can not run anymore. I have done the configuration for this motor, but it's still appear error message 300500: system error at 000BH & 0001H. The1PH motoris used withthe SIMODRIVE 611 POWER MODULE 1 axis,it's okey I think so but the put-in left extension that we had usefor 2 axis power module. I have attacheda descriptionfilefor details. The CCU 3.4 have 2 axis FSD. Is this the proroblem with my system? Thanks & Best Regards. TuanNA Attachmentattachment.pdf (205 Downloads) |
3/23/2009 6:58 AM | |
Posts: 4 Rating: (0) |
I have never used STEP7. I was doing it through HMI: start up->PLC then i trued changed the data |
Follow us on