1/27/2016 10:02 AM | |
Posts: 1 Rating: (0) |
how to use interupt procedure call in hsc 1 mode 10 and 9. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/27/2016 2:32:35 PMNew subject after splitting |
|
1/27/2016 3:12 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello arun; Have a look at TIP 04 from the S7-200 Tips and Tricks. These are a collection of various tasks (including sample code)that can be performed using a S7-200 PLC. with Microwin software, in various fields, such as communications, regulatory control, intehgrated functions, etc.. TIP 04 discusses How to use HSC; see the attached screenshot, which details the use of the interrupts with HSC instructions.. Download the Tips and Tricks from the following link: https://support.industry.siemens.com/cs/ww/en/view/1232912 Hope this helps, Daniel Chartier |
Follow us on