1/19/2020 8:52 AM | |
Posts: 9 Rating: (0) |
Hello all I have the same problem. I installed update 4 from TIA updater. Still having problem. When I go online, IE General is not connected and I receive these messages: Connection to IE general_1, via address IP=192.168.0.10, failed.,1/19/2020,10:58:42 AM Online: The connection to the target module cannot be established.,1/19/2020,10:58:42 AM any idea how to fix this?! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/20/2020 11:50:58New subject after splitting |
|
1/21/2020 6:20 AM | |
Posts: 9 Rating: (0) |
Hello I use TIA Portal v15.1 and WinCC runtime professional update4 and I added PC station for HMI screens. I practice on a PC with windows 10 enterprise, 64bit operating system. I am practicing on creating faceplate with "68014632_Faceplates_EngineeringExamples_en" documents. When I go online, IE General is not connected and I receive these messages and when I activate wincc runtime, the IO field doesn't show tags: Connection to IE general_1, via address IP=192.168.0.10, failed.,1/19/2020,10:58:42 AM Online: The connection to the target module cannot be established.,1/19/2020,10:58:42 AM I changed my CPU from 1200 to 1500 and everything was fine. why it can not be done by CPU 1200? I attached some screenshots of my PG/PC and the problem. How should I fix this problem? thanks in advance AttachmentConnectionProblem.zip (279 Downloads) |
Last edited by: Zahra_Kh at: 01/21/2020 06:22:00 |
|
Follow us on