5/13/2011 12:22 PM | |
Posts: 2964 Rating: (482)
|
Hello.... Pls. find thelinkof CP-5711 adaptor...... >>CP5711 adaptor works with CNC system with out 24V DC power supply unlike old adaptor. >>CP5711 adaptorr is useful with new laptops where PCIA slot is not available. http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6GK15711AA00&caller=view |
Last edited by: Ekalavya at: 5/13/2011 2:22 PM |
|
This contribution was helpful to2 thankful Users |
5/17/2011 4:38 PM | |
Posts: 2964 Rating: (482)
|
Hello..... There is further more information on CP5711. Update boot loader for CP 5711 If the CP 5711 is the last user in a PROFIBUS segment, there may under certain conditions be no power available for PROFIBUS termination. If the CP 5711 is the last user in a PROFIBUS segment with activated PROFIBUS termination at the PROFIBUS connector, there may under certain operating conditions be no power for termination. If no user applications (e.g. set STEP 7 or PG/PC interface) have been started, no power will be supplied for PROFIBUS termination:
http://support.automation.siemens.com/WW/view/en/49973488 Regards, Ekalavya |
Last edited by: Ekalavya at: 5/17/2011 4:39 PM |
|
This contribution was helpful to1 thankful Users |
2/2/2013 4:29 PM | |
Posts: 2964 Rating: (482)
|
Hello Caldas, Let me check it out...what error are you getting??? Regards, Prakash |
2/4/2013 12:13 PM | |
Joined: 9/10/2007 Last visit: 9/18/2024 Posts: 71 Rating: (1) |
Ekalavya The customer can work with STEP 7 but with the HMI Adv. not. The alarm 120202 is output. Thanks in advance. |
Follow us on