7/11/2013 2:33 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
It seems you have a SP only. Not the core of Microwin 4.0. Is it true? Best regards, Hristo Mihalev
|
7/11/2013 2:39 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello , i found following reply from one thread. Cann't Install Microwin V4.0 SP9
|
VANDE MATARAM..... |
|
This contribution was helpful to1 thankful Users |
7/12/2013 8:42 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
I don't know why is necessary to play around about installing of Microwin software. As in many other software their SPs and HFs are free downloadable. Like with Microwin. So, download the last available SP and update your existing version of software. By default to work with SP only is not possible. To make those tricks is it legal? If you have troubles with installation files just openSupport Request. In a short time you will receive a help. Best regards, Hristo Mihalev |
7/12/2013 11:00 AM | |
Joined: 2/8/2009 Last visit: 4/9/2024 Posts: 56 Rating: (3) |
Hi aanal, Thanks for this solution. I follwed your suggested steps. 1. I got microwin.exe files from my friend which already have installed microwin in her pc. 2. i copy this file in path C:\Program Files (x86)\Siemens\STEP 7-MicroWIN V4.0\bin 3. install STEP 7 Microwin V4 SP8 and SP9. which i had get from following link STEP 7 MicroWIN V4.0 SP8 and SP9 - Available for Download 4. follow the steps given in above site for first install MicrowinSP8 than remove Microwinsp8 and install MicrowinSP9 this work fine again thanks all of you guys. thanks lot for making my life simpler. |
8/7/2013 7:47 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, You need a full instalation CD/DVD to do the upgrade. How can you carry out an upgrade on an operating system that no longer supports the existing STEP 7 Micro/WIN version? If you don't have the Microwin CD, no upgrade needed. Just buy the full version. Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
3/26/2014 7:34 AM | |
Posts: 340 Rating: (6) |
new question is splittet to micro win and pc adapter error, cpu-226 cn |
1/7/2015 11:01 AM | |
Posts: 2 Rating: (0) |
This solution helped me out. I copied .exe, as specified by you. But it looks very strange for me. Thanks alot..
|
This contribution was helpful to1 thankful Users |
4/28/2017 12:30 PM | |
Posts: 2826 Rating: (684) |
|
This contribution was helpful to2 thankful Users |
2/2/2019 3:07 PM | |
Posts: 1 Rating: (0) |
iam experiencing the same too |
2/2/2019 3:32 PM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32878 Rating: (4064) |
That's not an accurate statement. What do you want to do exactly? |
10/29/2023 6:56 PM | |
Joined: 9/14/2023 Last visit: 4/4/2024 Posts: 1 Rating: (0) |
If you want 4.0 sp9, Do not install 4.0 sp8, install 4.0.6 first, and then install 4.0sp9. |
Follow us on