4/29/2019 1:24 PM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014) |
Hello, do you have the complete Ordernumber of the IPC? Regards Christoph |
4/29/2019 1:28 PM | |
Posts: 29 Rating: (0) |
Hi, i have no ordernumber. The device i work with, is an old one, which will not use productively anymore. Regards |
4/29/2019 1:29 PM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014) |
hello, no ordernumber on the typeplate? no number beginning wit 6AU...? Christoph |
4/29/2019 1:37 PM | |
Posts: 29 Rating: (0) |
My fault, sorry. 6ES7647-8AA60-1AA2 This one?! |
4/29/2019 2:08 PM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014) |
hello, yes this one. the sata power connectors are beside the batterieconnector on the mainboard. Regards Christoph |
4/29/2019 2:11 PM | |
Posts: 29 Rating: (0) |
Do you mean the white ones, with 5 or 4 pins? And i can use a "normal" ssd connected via SATA?! Do you try it ? |
4/29/2019 2:14 PM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014) |
Hello, yes this two i mean. My IPC227D here have a SSD inside and work without any problem. Regards Christoph |
Follow us on