4/22/2016 4:20 AM | |
Joined: 10/17/2007 Last visit: 4/17/2021 Posts: 2497 Rating:
|
What kind of CNC system do you have? if not sure check in control cabinet --take picture of system or find Siemens part# such as 6FC5357-0BB21-0AE0 is for SINUMERIK 840D POWER LINE NCU 572.2. if for this system you need 2 manuals at least , I cutting some key points attached just give your basic idea. It is trig user alarm by PLC in DB2 some bit. to display alarm# on the HMI, alarm text will save in HD of HMI under some path in special named file. so find system info 1st, then looking for manual
Attachment840D_al_tx.zip (33 Downloads) |
Last edited by: nulizhang at: 4/22/2016 4:41:14 AMPlease Help me to understand your question! |
|
4/25/2016 7:33 AM | |
Joined: 4/23/2010 Last visit: 4/21/2021 Posts: 6554 Rating:
|
Hello, PCU50.3 is basic control unit with HDD, Memory module & MCI board. Please read below manuals which gives basic information about, NC, PLC & drive commissioning. In CNC system, NC, PLC & HMI variables interface signals needs to set to define appropriate messages & alarms. SINUMERIK 840D sl Commissioning CNC: NC, PLC, DriveSINUMERIK 840D sl, NC variable and interface signals |
This contribution was helpful to
1 thankful Users |
4/26/2016 5:49 AM | |
Joined: 4/23/2010 Last visit: 4/21/2021 Posts: 6554 Rating:
|
You are welcome. |
This contribution was helpful to
1 thankful Users |
Follow us on