12/3/2020 10:04 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, 25202 is communication failuer & is similar as 25201. So you need to replace or get repaired Z axis drive. Yes you should take back up at particular interval & also keep original back up data (NC, PLC, Sinamics drives, Alarm text message text file etc. etc.) supplied by OEM or machine builder. Please refer Replacement of S120 componenets hint topic to understand component replacement. |
12/3/2020 12:05 PM | |
Posts: 20 Rating: (0) |
how to take back up of sinamic drive ? is it possible to take backup in 802d sl hard drive or have to take backup external pg? |
12/3/2020 12:30 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
802D SL does not have HDD. User can take back up on CF card or on USB drive or on external PG which need software & data cable. Please check tool box supplied along with system. This CD contains necessary software e.g. RCS 802 tool with which user can take back up on external PG/PC. Please refer attached sheets (extracted from Siemens manual) which will help you understand data back up procedure on different media. Its always recomanded to take series back up which will have all necessary data to start up machine in case data is lost. Also user can take individual back up of MPF, SPF program files, PLC, drive etc. etc. so that it can be restored as & when requred. HTH Attachment802D SL data back up.pdf (125 Downloads) |
12/4/2020 10:11 AM | |
Posts: 20 Rating: (0) |
How to take sinamic double module back up in pg using starter software sir? Which cable to use for communication? Which driver should use? |
Follow us on