4/27/2020 1:00 PM | |
Posts: 2964 Rating: (478)
|
Hello, NC memory is full... could be there is a file in part program directory by name NRK DUMP and NRK fault ? if it is there please delete this check? |
4/27/2020 4:21 PM | |
Posts: 9 Rating: (0) |
Hello, We got this machine recently and it was out of the power for 3 months. This resulted in data loss for PLC and NCK. Battery has been changed but whatsoever we can't start running due to this problem. The backups are from OEM, so they are factory backups and not previous owner's backups. From the previous owner, the engineer dismantling the machine used some software called 'CNC2000' to backup data, and the backup is in .CNC format - but this backup file doesn't even work for us, as it shows error DATA immediately on the beginning. So, that's why we requested factory backups. But now the memory not enough problem showed up. I'm attaching all these files in a zip, so maybe you or someone with knowledge can have a look into these and let me know if the problem is actually with the backup data. "What is the indication observed in NCU seven segment display?" - It shows up '6' after the NC/PLC reset procedure.(Photo inside zip) Attachmentbackups.zip (449 Downloads) |
Follow us on