7/26/2020 1:01 PM | |
Posts: 7 Rating: (0) |
|
7/26/2020 1:02 PM | |
Posts: 7 Rating: (0) |
|
7/26/2020 1:02 PM | |
Posts: 7 Rating: (0) |
|
7/26/2020 1:03 PM | |
Posts: 7 Rating: (0) |
|
7/26/2020 1:04 PM | |
Posts: 7 Rating: (0) |
|
7/27/2020 2:29 PM | |
Posts: 7 Rating: (0) |
THANKS Mr. Technology Team FOR YOUR RESPONSE , PLEASE COULD YOU EXPLAIN MORE, BECAUSE I AM BEGINNER IN SERVO SYSTEM. THANK YOU. |
7/28/2020 3:41 PM | |
Joined: 10/11/2006 Last visit: 5/7/2024 Posts: 5834 Rating: (790)
|
Hello, with Kv= 0 and Precontrol = 100% the position controller doesn't have influence. You get the setpoint e.g 10mm/s to the drive (Use control panel and move with 10mm/s), and you get a value from the encoder e.g 9,95 mm/s. (trace velocity and actualvelocity) So you settings are OK. If you get velocity = 10 mm/s and actualvelocity = 5,04 mm/s, you have to analyse the reason for this. So reference speed or the encoder settings doesn't fit. Please compare between setting in DO and TO. 3.2.5.4 Automatic transfer of drive and encoder parameters in the device https://support.industry.siemens.com/cs/ww/en/view/109749262 |
With best regards, |
|
Follow us on