8/24/2019 5:59 PM | |
Joined: 1/1/2017 Last visit: 4/22/2024 Posts: 329 Rating: (11) |
Dear Team, I've 04 nos of Scalance X204-2 connected to each other in an unmanaged way only on Profinet interface. The number of CPU's connected are 04 nos of 410-5H which are sharing each others data via these switches. Is it possible to configure Point-to-Point communication via these Scalances among the 04 nos of CPU's? It's to mention that the main system is PCS7 V9.0 SP1 & the software range used is Vistulization Topology. There are 02 nos of Host Devices connected to 06 nos of Thin Clients. Refer the architecture. Regards OmKris AttachmentSystem Arcitecture_As-Built_Rev.02.pdf (22 Downloads) |
Follow us on