3/7/2012 9:34 AM | |
Posts: 6 Rating: (0) |
Hi, perhaps not bother, but I think you can help me. I have a problem with the PC Adapter (USB) - 6ES7 901-3DB30-0XA0. I can not connect to the CPU 200,300,400 and can not set the PG / PC interface to USB. I use Win 7 Professional 32 - Step7, Win CC and other working perfectly. Could you help me? I do not know how to fix this problem. Thank you for your reply. Jan Seer Here are the pictures Attachmentpictures.zip (252 Downloads) |
3/7/2012 9:50 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, The cable you have there (multimastr PPI) is only for use with S7200 and Microwin-software, not for Step7, S7-300/400. http://support.automation.siemens.com/WW/view/en/12676750 Regards, Marcjan |
Last edited by: Marcjan at: 3/7/2012 9:53 AMProblem solved? |
|
3/7/2012 9:58 AM | |
Posts: 6 Rating: (0) |
Thank you for early reply, which usb cable need to connect CPU 300 and 400? 6ES7972-0CB20-0XA0? https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=14692974&caller=view |
Last edited by: Jan Seer at: 3/7/2012 10:02 AM |
|
3/7/2012 10:05 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, Yes with that cable you can connect to S7300/400 and S7200 as well. See http://support.automation.siemens.com/WW/view/en/14692974/td there are allso cards for in laptop: http://support.automation.siemens.com/WW/view/en/12297301 Regards, Marcjan |
Last edited by: Marcjan at: 3/7/2012 10:09 AMProblem solved? |
|
3/7/2012 10:08 AM | |
Posts: 6 Rating: (0) |
Thank you soooo much!You are my star for today. |
This contribution was helpful to1 thankful Users |
3/7/2012 10:20 AM | |
Joined: 8/31/2005 Last visit: 3/7/2024 Posts: 2197 Rating: (326) |
For S7-300/400 (PROFIBUS and MPI) you can use :
or you can use a CP (up to 12 Mbit):
|
|
|
This contribution was helpful to1 thankful Users |
Follow us on