2/18/2019 11:10 AM | |
Joined: 1/6/2009 Last visit: 4/12/2024 Posts: 132 Rating: (2) |
Hello nulizhange. The HMI is a PCU 20. Please see the photos attached in a zip file. Wait for your feedback.
Attachmentphotos.zip (59 Downloads) |
2/20/2019 5:43 PM | |
Joined: 1/6/2009 Last visit: 4/12/2024 Posts: 132 Rating: (2) |
Please check the photos atached of the HMI and the NC in the PLC. Today I will make more tests to test the simodrive anda the control drive. My problem for now it is try to find the manual of NCU 6FC5 357-0BH00-0XE1. In the HMI I try to load the NC backup and it gives an error with no code and no description. THe backup of PLC I was able to download throught HMI but when cames the moment to download the NC part says, can't reset NC. The process finish and if I try only to download only the NC file it returns an error but no description.
Attachmentphotos.zip (47 Downloads) |
Follow us on