11/10/2015 10:13 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, please check the version again and exactly! (provide a screen to clarify this!) V13.0 SP1 latest Update is UPD5. To simulate a S7-1200 you need PLCSIM V13.0 SP1 (Latest Update is UPD1 for PLCSIM V13.0 SP1) And you can only simulate a S7-1200 FW V4.x or above! Regards Christoph |
Last edited by: ChristophD at: 11/10/2015 10:14:18 AMLast edited by: ChristophD at: 11/10/2015 10:16:42 AM |
|
This contribution was helpful to
1 thankful Users |
11/11/2015 7:35 AM | |
Posts: 9 Rating:
|
hello but i have up6 please check |
Last edited by: danial balali at: 11/11/2015 7:36:09 AM |
|
12/8/2015 10:52 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by narayangonj is split to a separate thread with the subject TIA V13, Error 'Tahoma font is not installed'. Best regards |
12/24/2016 10:10 AM | |
Posts: 3 Rating:
|
Thanks, that was my problem as well! |
4/15/2017 11:09 PM | |
Posts: 1 Rating:
|
I also had the same problem and it was solved by changing the FW device to 4.0 thanks for all the help. |
Follow us on