2/15/2019 10:10 PM | |
Posts: 158 Rating: (1) |
Well under all block counts, size, etc...tells me I can't set to use w/ 0BA6 because "block name exceeds 8 characters...." I have verified 9 times that none of the block names is longer than 8 characters...what am I missing?? I need to get this program on a 0BA6. Attached is memory info LSC 8.2 windows 7 help! Mark Attachmentdata.pdf (374 Downloads) |
2/15/2019 11:04 PM | |
Joined: 12/27/2006 Last visit: 4/15/2024 Posts: 1196 Rating: (113) |
Open connections are NOT allowd in LOGO! Post the original programm .LSC hier, so we can look at it |
2/15/2019 11:16 PM | |
Posts: 158 Rating: (1) |
I don't have any 'open' connections...I replaced the 'X' coil with an 'M' and it didn't help, still says my block name is over 8 char.Attachmentprogramforforum.zip (361 Downloads) |
2/15/2019 11:32 PM | |
Posts: 158 Rating: (1) |
I have done this many times with other similar programs, so i know it can be done. |
2/16/2019 4:50 AM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32845 Rating: (4061)
|
I can not do that either. Please start a Support Request and send the program to Siemens. |
2/16/2019 6:16 AM | |
Joined: 10/20/2015 Last visit: 9/5/2023 Posts: 94 Rating: (19) |
Hello I managed in an "abnormal" way to convert it but I do not know if it works. Can someone tell me if can open it? *I suggest you next time use FBD. Attachmentmarkheuer.zip (333 Downloads) |
This contribution was helpful to1 thankful Users |
2/16/2019 6:40 AM | |
Joined: 10/20/2015 Last visit: 9/5/2023 Posts: 94 Rating: (19) |
Hello ixo. I am not sure if I can tell you that. It might be a problem.......for me at first..... |
2/16/2019 6:15 PM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32845 Rating: (4061)
|
If you correct the block name error (I have overlooked it despite multiple searches), the program still can not be converted to a 0BA6 program (as noted by Scorp, thanks). The strange thing is that he complains about an OR block B201, where there are no OR blocks in LAD. And there is also no block in LAD called "Bxxx". If you convert the program to FBD, you will find this (and other) OR block. From B201 there are different OR or AND blocks in FBD. And since the 0BA6 has only 200 blocks, you can not convert this program to a 0BA6 program. If you replace the blocks with the numbers greater than 200 in FBD against blocks with a smaller number, so that no block number greater than 200 exists, you can select a 0BA6 as a device and convert the program back to LAD. It can be concluded: LAD at the LOGO! is a bad, error-prone implementation of the programming language FBD of LOGO !. AttachmentLXL VFD 4.0 for 0BA6 for forumguy_0BA6.zip (245 Downloads) |
Last edited by: ixo65 at: 2/16/2019 6:17:17 PM |
|
This contribution was helpful to2 thankful Users |
2/16/2019 7:32 PM | |
Joined: 10/20/2015 Last visit: 9/5/2023 Posts: 94 Rating: (19) |
Hahaha... you are right. And I agree, for the LOGO! the programming language is FOR SURE FBD! |
2/19/2019 3:35 PM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32845 Rating: (4061)
|
There's a first time for everything.... |
Follow us on