4/17/2012 9:17 AM | |
Posts: 18 Rating: (1) |
Dear colleagues.... I experienced with S5 135U CPU 948 (3UA13 and 3UA23) when loading Flash Memorycard to CPU. After seconds I had my CPU went stop After I checked ISTACK, compare program and so on and I found the STEP5 program changed by itself. It's weird problem for me. Please look at image attached the comparison between program (file) and cpu program. I'll attached the STEP5 backup program if needed Please give me idea about it. regards, beard. note: I copied from existing EPROM (which is running correctly) then blow to new EPROM also I upload from running program then blow to EPROM also I blow EPROM using PG720P and Field PG, but my problem still remained. AttachmentFB115 Comparison.zip (219 Downloads) |
4/17/2012 9:42 AM | |
Posts: 18 Rating: (1) |
Additional info, here I attach also STEP5 backup program. AttachmentEPRORIST.zip (214 Downloads) |
4/17/2012 10:34 AM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
Hi beard , does that mean that the CPUworks with the previous old flash modulebut not with the new or now with none of them? Regards. |
Give us your feedback and show us your respect! |
|
4/17/2012 10:44 AM | |
Posts: 18 Rating: (1) |
TIBI68.... Now running with old eprom module (Add info: I supplied same order number with the old one) beard. |
Follow us on