5/2/2012 10:40 AM | |
Posts: 267 Rating: (22) |
Hello, change the "Pulses per motor revolution" from 3600 to 360 in the "Extended parameters" of the "Configuration" of Motion Technology object. Do you know the CE-X7: http://support.automation.siemens.com/WW/view/en/38391227 |
5/2/2012 8:34 PM | |
Posts: 272 Rating: (4) |
you will get the counts in the Hardware ID...you will have to reset it using a write function.... |
5/2/2012 9:15 PM | |
Posts: 89 Rating: (16) |
You(all) are right, I should stay away of this forum |
Follow us on