11/30/2007 3:03 PM | |
Posts: 101 Rating: (11) |
Hi Fran, Take a look at this thread: /tf/WW/en/Posts/2120 Also, at these links, they might be of help: http://www.airborn.com.au/rs232.html http://www.airborn.com.au/rs585.html http://interface.centraltreasure.com/rs485.html http://www.commfront.com/RS232-RS485-RS422-Serial-Converters/RS232-RS485-Converter.htm?gclid=CIWqnabdhJACFSdWZwod1S4hrw |
12/4/2007 10:17 AM | |
Posts: 26 Rating: (1) |
Hi Husam !. Thank you for your answer but I think it ismore a signal/wiring problem than a power management one. My RS485 converter has an external power supply. It doesn't take power from the RS232 port. Here you are the user's manual of the Aten converter. I send you too a screenshot from the communications screenof MicroWIN that i get when trying to communicate the PLC with the PC via the Aten converter and my homemade cable. This result is the same even if i unplug the PLC from the converter. I think the converter (or the cable i made) is working in test mode. AttachmentAten.zip (347 Downloads) |
12/4/2007 12:10 PM | |
Joined: 12/4/2007 Last visit: 5/21/2024 Posts: 8 Rating: (0) |
Hi Fran, |
12/6/2009 2:33 PM | |
Posts: 1 Rating: (0) |
following links,hope will help someones : http://www.sintech.cn/en/rs232%20rs485%20converter/rs232%20rs485%20converter.htm and http://www.shopsintech.com/index.php?cPath=3&osCsid=433ac6dd26d2c115a7610a39a74fc0df. |
7/24/2011 1:20 AM | |
Posts: 4 Rating: (0) |
Sounds like you are using a RS232 to RS422 covnerter instead of a [url=http://www.usconverters.com/index.php?main_page=index&cPath=65]RS232 to RS485 converter[/url], the RS422 converter has 4 wires where the RS485 only has 2 data wires. Check this basic [url=http://www.rs232-to-rs485.com]RS232 to RS485 converter[/url] wiki, it will help you with the basics. |
Follow us on