11/16/2011 10:04 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Hi , For the first time I have to work with an S5 PLC, The prgrm is written in STL of course , my question is does anyone has a list with all operands etc for STL in S5. I've got the one for S7 but I can't find everything back in this document... I think some of the operands and functions of S5 aren't present anymore in S7. Attachment : S7-list AttachmentSTL-cheat-sheet-by-category.pdf (2237 Downloads) |
This contribution was helpful to1 thankful Users |
11/16/2011 11:12 AM | |
Posts: 376 Rating: (57) |
Hello S7-FreshMan, you find such lists in the manual “Programming Instructions” of the respective SIMATIC S5-PLC. Or in the respective operation list of the S5-PLC typ. Perhaps helps you also the list in the manual SIMATIC “STEP 7 V5.5 From S5 to S7 “. Look at the chapter Appendix, Address and Instruction Lists Here the Link: http://support.automation.siemens.com/WW/view/en/45531547 Question. What kind of SIMATIC S5 PLC do you use? Best regards Azteke0110 |
This contribution was helpful to1 thankful Users |
11/17/2011 9:28 AM | |
Posts: 376 Rating: (57) |
Hello S7-FreshMan, As an example I send you the operation list of the S5-PLC system S5-135U. Look into the file attachment (pdf-file). S5-135U_Operations_List.pdf Best regards Azteke0110 AttachmentS5-135U_Operations_List.pdf (1891 Downloads) |
This contribution was helpful to3 thankful Users |
11/18/2011 11:14 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Hi Azteke0110 , thanks a lot for the information, the S5-plc's are from the next type : S5-95U & S5-115U. |
11/18/2011 12:28 PM | |
Posts: 376 Rating: (57) |
Hi S7-FreshMan, in the Siemens Service&Support sides you find the System Manual for the PLC-Type S5-90U/S5-95U. The Entry ID is 1091648. Here the direct Link: http://support.automation.siemens.com/WW/view/en/1091648 Please look into the chapter 8. And here the Link for the manual“S5-115U Programmable Controller CPU 941/942/943/944 Reference Guide“. http://support.automation.siemens.com/WW/view/en/1085938 In the Siemens Service&Support sides you find more manuals for SIMATIC S5 PLCs. http://Support.automation.siemens.com
|
12/24/2013 7:28 AM | |
Posts: 1 Rating: (0) |
Thanks for the upload... |
Follow us on