2/2/2016 9:28 AM | |
Posts: 68 Rating:
|
Hey guys, As you can tell i'm trying upgrade S5 CPU (115U) to S7 300 I have one "trouble making" DI card 6ES5 434-7LA12. I manged to see some PDF's regarding this card and as far as I can tell this DI card uses 2 byes, the first byte is the actual sensor connected to the card and the 2nd byte is for alarms in FC 2 and also it has a reset wired in the card. I want to rewrite the logic in different FC instead of the DI card 6ES5 434-7LA12 and thats the part where I need your help. Can you please advise me what to? FYI I attached the FC and HW config from the S5 IO AttachmentHW Config.rar (33 Downloads) |
Last edited by: woop_ass at: 2/2/2016 10:01:13 AMLast edited by: woop_ass at: 2/2/2016 10:02:56 AM |
|
Follow us on