5/12/2006 9:17 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hello, You should import the GSD file of the EM277 into Step7. http://support.automation.siemens.com/WW/view/en/2615830 Assign it to the Profibus DP segment and configure the input/output module. Als configure the I/O offset in the V-memory (S7-200). At the S7-300 you communicate through the Inputs and Outputs assigned. And in the S7-200 you communicate through the V-memory Hope this will help. Wizard |
5/17/2006 9:36 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hi Mojo, I' m happy to hear the information was usefull. Greetings, Wizard |
Follow us on