6/13/2021 5:05 PM | |
Joined: 6/24/2010 Last visit: 11/9/2022 Posts: 4 Rating: (0) |
After power failure, the S7-410-5H RACK 1 shows the EXT F and BUS F leds on, attached are the Diagnostic Buffer for both Racks. The IM153-2 redundant modules shows BUSF1 and BUF2 leds on. I see in several IM153-2 both channels with BUSF1 and BUSF2 leds on too. The S7-410 5H has EXT F fault it means the failure is in the S7-300 hardware, can you support me in order to find the problem in the HW structure. AttachmentS7-410 5H Diagnostic Buffer.zip (356 Downloads) |
Last edited by: Edegel1 at: 06/16/2021 03:55:20After power OFF and back to power ON both PSU, the CPU restart without issues. thanks for your attention. |
|
Follow us on