2/22/2016 9:55 AM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
any help? |
2/22/2016 10:01 AM | |
Posts: 1529 Rating: (202) |
What controller are you using? The functionality is probably built in. |
2/22/2016 11:21 AM | |
Posts: 1529 Rating: (202) |
Set pulses on what? |
2/22/2016 11:52 AM | |
Posts: 1529 Rating: (202) |
WHAT PLC ARE YOU USING??????????????????????????????????????? Third time asking |
2/22/2016 11:59 AM | |
Posts: 1529 Rating: (202) |
Download the S71200 Motion Control manual and read it. What you want to do is very easy. |
2/22/2016 12:15 PM | |
Posts: 1529 Rating: (202) |
Let me guess, this is some sort of school project. |
2/24/2016 5:20 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
it is dc geared motor from Nidec 404.961 it has hall effect sensor which gives pulses.in my configuration i haven't used the feedback yet. I configured the axis technology and I used its commands, I downloaded the program to the PLC and I push start but i didn't get output from PTO. However when I configure it to PWM it gives output. the whole program is activated except the CTr_PWM and Move absolute. I neither used any limit switches in hardware nor software the attached file shows the program and axis configuration.
AttachmentDoc1.pdf (367 Downloads) |
Last edited by: engma at: 2/24/2016 5:22:56 PMLast edited by: engma at: 2/24/2016 7:08:35 PM |
|
2/24/2016 9:42 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Did you try moving it manually trough the "commissioning" control? |
2/25/2016 6:45 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
I didn't connect any drive, I will use simple H-bridge to drive the dc motor. Is it obligatory to connect the drive ? it gives light with PWM without connecting any output or drive. I activated manual control but the commands weren't activated as shown in pic.
AttachmentDoc1.pdf (389 Downloads) |
Last edited by: engma at: 2/25/2016 6:48:24 PMLast edited by: engma at: 2/25/2016 6:51:15 PMLast edited by: engma at: 2/25/2016 6:57:40 PMLast edited by: engma at: 2/25/2016 7:20:22 PM |
|
2/25/2016 8:39 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Take the device offline |
2/25/2016 9:30 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
ok, I will my version is v13 sp1 |
2/25/2016 10:24 PM | |
Posts: 5225 Rating: (1192)
|
(1) (2) The MC_POWER should not be activated if you try to use the commissioning tool. I recommend strongly to use this tool to experiment with the JOG function to see the results. (3) (4) (5) A PWM can be used to vary the power / speed via the H-bridge. That means that a ramp up - run - ramp down profile can be generated with the aim to do positioning. Speed is the tool used to do positioning. When using a PWM, a mathematical formula and some rule based control is needed to regulate the speed to achieve position according to a position setpoint and position feedback. now.... you are in control of your own project and this thread - Kind regards. AttachmentDoc1 with commentary.pdf (343 Downloads) |
Last edited by: William_B at: 2/26/2016 7:20:29 AMAdd document with commentary for clarity. Original document posted {2/24/2016 5:20 PM}. |
|
2/25/2016 10:46 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
Dear William I am sorry, after your great post it is still not clear for me what is the problem with my program. Is it enable or move absolute ...? I will apply the pulses to the gate of transistor drive the motor .the driver is some thing like that http://store.fut-electronics.com/collections/dc-motor-driver/products/dc-motor-driver-30a
|
Last edited by: engma at: 2/25/2016 10:47:10 PMLast edited by: engma at: 2/25/2016 10:48:13 PMLast edited by: engma at: 2/25/2016 10:50:41 PMLast edited by: engma at: 2/25/2016 10:55:42 PM |
|
Follow us on