7/26/2019 3:28 PM | |
Posts: 9 Rating: (0) |
Hello I am trying to connect to the iot2040 using X30/X31 I have used this usb adapter and a cross-over cable but when I try to connect with putty or Tera Term I only get a blank screen. The baud rate is set to 9600 which I believe is correct. Both X30 and X31 are set to RS232. I have checked that the cable is working ok with other devices. I can use ssh with no problems but need to use the COM port instead from now on as I need X1 and X2 ports to be free for something else. Is there anything I need to configure and is the usb adapter that I am using suitable? Thank you |
7/26/2019 3:39 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, To setup a serial communication over putty you need an FTDI cable and drivers. You then connect it to the X14 interface and set the Baudrate to 115200. Kind regards! |
7/26/2019 4:26 PM | |
Posts: 9 Rating: (0) |
Thank you Fe_lipe so just to confirm I cannot use X3x ports to connect via putty and must always use X14. |
7/29/2019 10:34 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Yes exactly. You have to use X14. Kind regards! |
This contribution was helpful to1 thankful Users |
Follow us on