9/12/2018 6:56 PM | |
Joined: 9/27/2006 Last visit: 9/23/2024 Posts: 12282 Rating: (2685) |
Hello mmkhan; Do you mean you have purchased one (a single) Profibus connecter for this project? You need 2, one connected to the PLC programming port, the other on the HMI Profibus port; you require a length of Profibus cable between the 2; that is why there are those 2-wire Jack's in the connector; do not forget to crimp the cable shield in the connector clamps. See the attachment below. You connect the PPI programming cable on the piggy-back that is on the backside of the connector you have placed on the PLC programming port. Hope this helps, Daniel Chartier AttachmentWiring Profibus cable and connector.pdf (299 Downloads) |
Last edited by: dchartier at: 9/12/2018 7:04:10 PM |
|
9/12/2018 8:36 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, what have purchased this? Or....
|
9/18/2018 7:48 PM | |
Joined: 9/28/2007 Last visit: 2/20/2024 Posts: 234 Rating: (12) |
Dear Dchartire sorry for disturb you.. actually i have only one profibus connector which you and other mentio earlier.. second i am using normal PPI cablr and microwin software for communicating.. i connect my PPI cable on piggy back connector and connector other side on plc cpu and profibus cable from HMI connect of red and green wire on connector.. HMI and PLC cpu communicating well but when i want to go online with CPU it show no error but did not detect any CPU . just like attachment .. actually i early told you i want to see online data transmitting between CPU(222CN) and HMI(Smart line 700IE).. SEE attached file and help me... . Attachmenterror.zip (287 Downloads) |
Muhammad Munir |
|
Follow us on