6/1/2009 6:30 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi do as per the attachment and you will be able to boot the 802D normally regards Ram Attachmentstartup 802d.pdf (1038 Downloads) |
This contribution was helpful to1 thankful Users |
6/1/2009 8:24 AM | |
Posts: 22 Rating: (1) |
Hi Thanks for help . I followed the procedure for START UP. After reboot with default data, appears the same screen that was sent. Iri |
6/1/2009 9:02 AM | |
Posts: 63 Rating: (3) |
Hi , it needs Sys. software updation. |
6/1/2009 10:46 AM | |
Posts: 22 Rating: (1) |
Hi How can I do this? Please tell me the steps you need to follow. Thanks Iri |
6/18/2009 12:29 PM | |
Posts: 22 Rating: (1) |
Hi, I did not System software of 802D V2.4.3. But I have System software of 802D V2.2.6.Using this cardware software write with system software of 802D V2.2.6 I am given the option of system software update. After that the system boot normally.Then I dowloaded the START_UP data and PLC programm. Everything is in order. The machine works.I need to change the PLC programm (is the first commissoning) and then to dowload again. Dowload was successful.The PLC is placed in RUN. On the screen appears image attached.In this situation, if reinstall the system software of 802D and reload the Start-up data and the PLC programm with the changes, the machine works. Where is the problem? Iri Attachmentfault1.pdf (645 Downloads) |
6/22/2009 7:04 AM | |
Posts: 22 Rating: (1) |
Hi, This problem occurs only after the restore PLC in RUN. Thank Iri |
This contribution was helpful to1 thankful Users |
Follow us on