5/11/2019 1:57 AM | |
Posts: 3 Rating: (0) |
Here is the card with red leds |
5/11/2019 2:00 AM | |
Posts: 3 Rating: (0) |
And the control number |
5/11/2019 8:50 AM | |
Joined: 10/27/2009 Last visit: 3/15/2024 Posts: 455 Rating: (77) |
"Input" + 8 is not sufficient to get the control back to live... You need to format the memory completely before. ("cancel" + 2 / + 3 / + 4) see chapter 2.2 in that document. position of switch S1 need to be checked for that operation as well. |
hope that helps |
|
This contribution was helpful to1 thankful Users |
Follow us on