7/3/2012 3:28 AM | |
Joined: 12/15/2011 Last visit: 4/17/2024 Posts: 2 Rating: (0) |
Hi Marcjan,' Ithink Ihave the same problem. I'm running Windows 7 Ultimate x64 SP1 on a Acer Aspire, 8GB Ram, Intel i5 Core. I installed Simatic Step 7 V5.5 SP1 and updated to SP2. Step 7 was working right. Last week I installed Micro/Win V4.0 SP9. After reboot the PC, I opened MicroWin and I received a message from Windows 7 (Pic SINEC.gif) when trying to choose the "Access Point" = invalid registry. After that I opened the Step 7 and I was not more able to communicate with S7-300 through "PC adapter USB" neither trhough Ethernet, with the message = "SIN_SERV.EXE not started". !!??!! So I unistalled and installed again MicroWin several times following differents posts. At the moment Step 7 looks like working good, but with MicroWin I don't ghe to set the communication interface/cable, when I try to install the PPI protocol the "Access point" does not shows any MicroWin driver (PC Adapter PPI)...... ??? During the installation no windows appear to set the Access Point for MicroWin. But in the Windows 7 list of Diveces under "SIMATIC NET", appear "SIMATIC PPI Transport". Have I some chance to run MicroWin SP9 in my Windows? Thanks. Attachmentsin_serv.zip (1641 Downloads) |
Last edited by: O_Moderator at: 7/3/2012 7:57 AMattachment converted to correct zip-file |
|
4/30/2013 4:28 PM | |
Posts: 5225 Rating: (1185) |
My issues were solved when looking at this post.. /tf/WW/en/Posts/81753 |
Follow us on