11/19/2021 5:15 PM | |
Joined: 9/28/2020 Last visit: 8/13/2024 Posts: 19 Rating: (0) |
Hello, a while ago you helped with the Logo and Victron. now I want the following the Cerbo has a start function for a generator. you can choose to start the generator when the inverter goes into overload. now I want to switch Q1 of my logo when the generator is started because of an overload .
I have my configuration in the attachment, could you take a look at it? thanks in advance ------------------------------------------------------------------------------------------ Attachmentoverload.zip (498 Downloads) |
Last edited by: Jen_Moderator at: 11/22/2021 09:11:34New subject after splitting |
|
11/19/2021 5:33 PM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33833 Rating: (4205)
|
Who should help you without precise details? Why did you set a gain of 0.01? Why is the ON value at 9? |
11/19/2021 8:44 PM | |
Joined: 12/18/2014 Last visit: 9/24/2024 Posts: 33833 Rating: (4205)
|
Are you sure that you must need the offset? I don't know it. Try to read register 3501 and not 3502. |
Follow us on