5/2/2020 2:31 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (267) |
Hello Autogen, For pcs7 IPC, when you set up, you must follow the IPC Restore procedure. 1. When you restore, it will ask you to configure the time, language, administrator name. 2. Then login to the windows, you should wait and do nothing at all (when the system configuration active is still at the top of the desktop) 3. About 5 to 10minutes waiting time, when everything loaded completely, licenses agreement term and condition will pop out and ask you to agree on sth. 4. then the system config active will ask you to change your computer name. 5. After changing the computer name to the final name, the windows will ask you to do a restart. You can restart it. 6. After a restart, if the system configuration active is still there, you must wait again. It will pop out "restart the computer" or "Do you want to install management agent?" 7. if the restart the computer dialog pop out, go ahead and restart the computer again. 8. if the management agent dialog pop out, for OS server, clients, ph, is, OPC , click yes. For Domain controller (follow compendium f) press no. 9. wait for 5 minutes, the system config will be completed and you are free to do anything you want. Yes, troublesome. but this is the way. If now you restart and nothing change, please use the IPC restore and restore back the original delivered version and do everything again. Hope this is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on