12/30/2011 7:05 AM | |
Joined: 8/25/2006 Last visit: 4/19/2024 Posts: 2203 Rating: (277)
|
Hello. T400 contain program suitable for different types of shears and drum shear is one of them. As I know you will also need a secondencoder at material side (which measures speed and position of material) and a light barrier. Look at manual, where you will find typical configurations, hardware connections and all parameters. |
12/30/2011 7:21 AM | |
Posts: 22 Rating: (0) |
Please find the attachment
Attachment2011-12-29 14_52_19.zip (355 Downloads) |
This contribution was helpful to1 thankful Users |
1/4/2012 2:43 PM | |
Joined: 8/31/2005 Last visit: 3/7/2024 Posts: 2197 Rating: (326)
|
The normal orderin the rack is: CUx - CBx - T400, or without a communication module: CU - empty - T400
Please tell us more detail on the LEDs: Have a look on the "brief description" onpage 16 in the document,onpage 18in PDF. |
|
|
1/6/2012 6:56 PM | |
Posts: 22 Rating: (0) |
Please help!!!! |
1/9/2012 11:01 AM | |
Joined: 8/25/2006 Last visit: 4/19/2024 Posts: 2203 Rating: (277)
|
Hello. A097 is alarm from communication board. Look for its decription in the manual, chapter 3.3.1. |
Follow us on