Industry Online Support
Technical Forum
5/18/2010 12:12 PM | |
Posts: 2 Rating: (0) |
Hey all. I have some problems. I'm pretty new at Step 7, PLCSIM, etc. My problem is that I don't have a hardware to test it, so my only option is PLCSIM. Now I would like to know if there is any option to run simulation on PLCSIM on PC #1 and connect to that simulation from PC #2? I have configured the simulation like so:CPU 315-2 DP with CP 343-1 TCP. On CP a have configured an IP 192.168.0.30 which is the same as on PC #1. Is that correct? How should I configure PG/PC Interface? Is it even possible to connect to this simulation from other computer (for example PC #2)? Is it possible with libnodave (v0.8.4.5)? As you probably noticed on my PC #1 is Windows (XP) OS, and on PC #2 is Linux (Ubuntu)... I have attached my project if someone will take a look. Thanks for help, Uros AttachmentS7_300.zip (315 Downloads) |
Follow us on