9/7/2020 2:25 PM | |
Joined: 3/17/2015 Last visit: 8/30/2024 Posts: 5 Rating: (0) |
replace a CPU 417-4h to a CPU 410-5H, once the hadware was compiled and downloaded, I proceeded to download the user program (OBs, FBs, FCs), it threw me the following message:"unable to copy the block". And it happens that I cannot download the program to the CPU, I was inquiring through siemens support, I found the following: “The download you are trying to download is a STEP 7 mechanism that is blocked for the CPU 410-5h that only downloads with PCS7 (CFC) (therefore it works for CPU 417-4H and not for CPU 410). " If this is the case, how can I download the user program (ob, fc, fb) should there be a procedure to download the program or some hotfix that allows downloading in step 7 in this type of CPU 410-5H. Regards RSG ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/08/2020 06:21:53New subject after splitting |
|
9/8/2020 6:22 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
|
Follow us on