1/21/2022 11:26 PM | |
Joined: 9/27/2006 Last visit: 5/8/2024 Posts: 12257 Rating: (2666)
|
Hello EVauto; Based on the contents of the docuent you refered to, the information you seek is not included in the Modbus mapping of the VerciCharge: https://support.industry.siemens.com/cs/ww/en/view/109802027 However, the VersaCharge operating manual shows status LEDs on the module face that indicate whether a vehicle is connected to the charger (and various other condftions) that could give you this information, if it os possible to read them through the reserved registers in the mapping. I would expect a manuafacturer to wnt to have access to remote daigsostics for such distrbuted grid equipment. https://www2.unbc.ca/sites/default/files/sections/green/versichargeoperationsmanual.pdf The only ones who could be able to answer such questions as you have would be the Siemens division that designs the chargers. The operating manual for the charger shows the contact links for the techs in that division, see the screenshot below. Hope this helps, Daniel Chartier |
8/26/2022 9:49 AM | |
Joined: 7/1/2022 Last visit: 5/9/2023 Posts: 2 Rating: (0) |
Where can I download the modbus map? The given download link doesn't work. |
8/26/2022 2:15 PM | |
Joined: 9/27/2006 Last visit: 5/8/2024 Posts: 12257 Rating: (2666)
|
Hello Matthias; You are right, many of the documents discussing the Versicharge Modbus mapping that were available last January seem t have been removed from the web. One of the remaining ones has this indication: https://www.lukuexpert.ee/et/e-pood?action=download&picture_id=22825, Section 5.3.5, on page 45 : “Modbus map The Modbus map is available on request from the Download Center" It is also difficult to locate the Versicharge Download Center these days. The best alternative might be to follow the Contact Us link in this webpage: https://siemens.com/versicharge Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 08/26/2022 14:17:57 |
|
Follow us on