9/10/2014 9:25 AM | |
Joined: 10/7/2005 Last visit: 4/23/2024 Posts: 3004 Rating: (1046)
|
Hello YKW 4096 Bytes is the I/O limit of the CP443-5 Ext (see CP tech spec HERE) and my guess is that you are trying to exceed this. As these 4096 Bytes can be "scattered" across a large overall address range, only you can check ifyou reached thislimit (mind you, HWconfig should have issued you with a popup informing you that you exceeded the 4096 I/O Byte limit, did you get this warning?). Let's say you reached the limit, what you can do is this: - Add another CP443-5 and put the extra DP Slaves on it - Use the CPU's on-board DP port if you need all these DP Slaves on one port (it can handle 8192 Bytes for a current 416-2, please see tech spec of your CPU for more). I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on