8/18/2015 10:59 AM | |
Joined: 10/1/2013 Last visit: 4/25/2024 Posts: 605 Rating: (71) |
Hi, you can use the 1SI module of the ET 200S and connect readers by RS422 cables. Here is an application example with code blocks for this solution: If you want to use others readers than RF600 (which could be RF200/RF300) you need to use the communication module RF180C which can be connected via PROFINET. And to this communication module you can connect any RS422 readers. For the last two solutions you should use the ident profile instructions. Do you have STEP 7 V5.5 or TIA Portal? |
Last edited by: Owei at: 8/18/2015 11:01:31 AMLast edited by: Owei at: 8/18/2015 11:05:39 AM |
|
8/18/2015 1:24 PM | |
Joined: 10/1/2013 Last visit: 4/25/2024 Posts: 605 Rating: (71) |
you're welcome :) |
8/18/2015 1:41 PM | |
Posts: 4 Rating: (0) |
Ok, so I have just one question. By RS422, using modules, I can connect ANY RFID reader, not ONLY Siemens? I understand this corectly or not? |
8/18/2015 7:35 PM | |
Posts: 4 Rating: (0) |
Ok, now I know exactly what I want. Thanks a lot once again |
This contribution was helpful to1 thankful Users |
Follow us on