8/6/2020 2:34 PM | |
Joined: 12/11/2018 Last visit: 1/2/2024 Posts: 26 Rating: (0) |
Hi , i don´t know, if someone can Help me. - i want to write a warning message, which should display on my TP 1900. So i have a tia v16 and i already programm a Variable, which a Boolean status. i need, that when the Variable is true, the my Warning appears on the Screen and if the Variable is false, my warning disappear. How to realise it? i use UDT as Datatyp - The next question is that, i have a Text list.In this Text list i have Variable with the name Text_1 and this Variable has the selction Value/range. The variable Text_1 content differents others Variable in The Text list entries. There i have for each Text a value number before. The question ist, how can i read this Text_Messages in my Programm by calling the Value Number corresponding in ? e.g if it looks like this default value Text 506 Good morning everyone i need that in my programm i call the 506 and it comes with the text Good morning everyone. Is it possible? Kind Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/07/2020 08:26:45Neue Überschrift nach Splitten |
|
8/7/2020 7:26 AM | |
Joined: 7/5/2013 Last visit: 9/19/2024 Posts: 3112 Rating: (512) |
Hello Maestro, have a look in the manual SIMATIC STEP 7 Basic/Professional V15.1 and SIMATIC WinCC V15.1, section "Output of texts from a text list in an alarm (Basic Panels, Panels, Comfort Panels, RT Advanced)". Besides, you have to use a word resp. int tag for triggering alarms and use one bit per alarm. Regards, Frink |
Pi is exactly three! |
|
Follow us on