9/24/2015 10:03 AM | |
Joined: 9/29/2011 Last visit: 4/22/2024 Posts: 23 Rating: (5) |
We are suffering the same problem.A vocational training school with the two plcs S7200 and S71200. After updating to new TIA V13 SP1, Microwin can not communicate. The software runs OK but you can get online with the PLC. The problem only happen in Windows 7 64 bits. Is there no solution for this problem? Reinstall SO and then dont use the TIA V13 SP1 is a mesh. We solved with another mesh that is use Microwin 4.0 SP9 in a virtual machine in order to communicate with the real PLC with our old PC/PPI cables. It is disgusting! Siemens software, what more can I say. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/24/2015 3:07:37 PMNew subject after splitting |
|
9/24/2015 3:25 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, have you seen this Thread. Scroll down to luciferC4´s post and download the attachment "PCPPIcable.zip". It is the very last post on the first page. Try to install it as Admin. I think its a try worth hope it helps, regards, |
FCK WAR! |
|
9/24/2015 7:02 PM | |
Joined: 9/29/2011 Last visit: 4/22/2024 Posts: 23 Rating: (5) |
hi mop, thanks for your reply
I've already tried this option and it doesn't work in my case. |
9/30/2015 1:44 PM | |
Joined: 9/29/2011 Last visit: 4/22/2024 Posts: 23 Rating: (5) |
Problem fixed, |
This contribution was helpful to1 thankful Users |
Follow us on