11/17/2016 5:53 AM | |
Joined: 4/28/2015 Last visit: 4/26/2024 Posts: 11 Rating: (0) |
Hi Jurgen, How is the continuation of this problem? Is it solved? I also face the same problem with the same PCS version in my client's ES. Started around three months ago and it is getting more and more frequent lately. This problem already caused the Multiproject to be corrupt due to sudden restart in the middle of program modification. If anyone know how to fix this problem, please let me know. Regards, Freddy ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 17.11.2016 10:37:51Contact data deleted Last edited by: Min_Moderator at: 28.03.2017 14:53:00Neue Überschrift nach Splitten Last edited by: Min_Moderator at: 3/28/2017 2:53:45 PMAdd quote |
|
11/21/2016 7:14 AM | |
Posts: 567 Rating: (106) |
Hi, I trink you just have to configure a valid ip adress and than it should work. |
3/29/2017 3:50 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
I faced the same kind of issues few years back. My problem was happened on PCS 7 V8.0 Sp1. There are one set of OS servers using Intel type of servers. The network was in domain group. The issue was, the network adapter will suddenly shutdown and disable. Then, we will need to restart the station. This happened to not only server stations , but engineering server as well. only client station was fine. These were the items i checked, 1. antivirus, compatibility 2. IT related settings 3. IP Configuration 4. model ( the server is intel brand , and the ES is dell) 5. Security ( apply security setting) Then i wasted a lot of time to check on the window event logs ( Computer management-> window logs) I also checked on all the log files in (C:\Program Files (x86)\SIEMENS\WINCC\diagnose) . And till now, the problem is still exist. We doubted on the IT related setting might not be the PCS 7 recommended settings. And now, they were used to the restart of the system and became a maintenance routine for them. they will shutdown station once a month. From now on, i preferred to propose customer to purchase siemens workstation, as they will pre-configured all the settings that were suppose to be configured. I seldom faced network or strange behavior when customer using Siemens workstations. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on