04.08.2010 13:34 | |
Beigetreten: 21.03.2006 Letzter Bes: 10.09.2024 Beiträge: 10228 Bewertung: (1181) |
Hotfix1 fur SP5. Hotfix 1(K5.4.5.1) for STEP 7 V5.4 SP5 What has Changed Compared to Version STEP 7 V5.4 SP5? HWConfig • As of this Hotfix: The "Save and Compile" function has been improved. • As of this Hotfix: The consistency check of stations with CiR objects and I/O maximum expansion has been improved. • As of this Hotfix: The dialog for entering the update time in the project properties of the PROFINET IO system has been improved. • As of this Hotfix: The import of stations with normdevices has been improved. CPU Messages • As of this Hotfix: The creation of new messages has been improved. ... Dieser hotfix ist schließen darin ein STEP7 Professional 2006 SR6... Wenn wir in zu demselben fortsetzen... Hotfix3 fur Step7 5.4 SP5 What has Changed HotFix3 Compared to Version STEP 7 V5.4 SP5? HWConfig • The "Save and Compile" function has been improved. • The consistency check of stations with CiR objects and I/O maximum expansion has been improved. • The dialog for entering the update time in the project properties of the PROFINET IO system has been improved. • The import of stations with normdevices has been improved. • The handling of cyclic interrupts for an improved interoperability with the fail-safe configuration pack has been expanded. • Monitoring of inputs and outputs is now also supported for CP1616 V2.4. • As of this Hotfix: The compatibility in case of bandwidth violations with IRT has been improved. • As of this Hotfix: Configuration of the CP343-1 ERPC is now supported. CPU Messages • The creation of new messages has been improved. NetPro • As of this Hotfix: The slot view for S7 connections with CP343-1 has been improved. RSE • As of this Hotfix: The handling of GSDML files has become more stable. • As of this Hotfix: Processing of messages from previous versions has been improved. S7-PCT • As of this Hotfix: Configuration of S7-PCT has been extended. S7-PCT now supports a standalone mode and you can call it up directly from the MS Windows Start menu. Und HotFix4 for STEP7 V5.4+SP5 http://support.automation.siemens.com/WW/view/en/41173255 http://support.automation.siemens.com/WW/llisapi.dll/csfetch/41173255/S7Sp5Hf4.zip |
Zuletzt bearbeitet von: UMENCHO am: 04.08.2010 13:42Zuletzt bearbeitet von: UMENCHO am: 04.08.2010 13:41Zuletzt bearbeitet von: UMENCHO am: 04.08.2010 13:40 |
|
Für diesen Beitrag bedanken sich1 Benutzer |
Folgen Sie uns auf