3/20/2021 10:45 AM | |
Joined: 12/7/2011 Last visit: 4/29/2024 Posts: 384 Rating: (9) |
Hi to everyone, I've migrated a PCS7 7.0 to PCS7 9.0, the system has the CEMAT v7.0 SP1 library too. Everything works fine, except for the CEMAT faceplate that doesn't pop up in the servers only. Looking for some problem i found something i don't understand. When install the CEMAT library, the default path is D:\CEMAT_CS, and i've installed there in all machines. I've runned the project update script in all machines without problem, but when i've checked the WinCC projects i found that: In the clients: the Application was D:CEMAT_CS\BIN\Scan_CS.exe and Work Directory D:CEMAT_CS\BIN.. In the servers:the Application was D:CEM_V6_CS\BIN\Scan_CS.exe and Work Directory D:CEM_V6\BIN First of all, in the servers i've tried to set the same path i found in the clients, but problem is still there, then i've tried to copy and paste the CEMAT_CS folder and renamed as CEM_V6, but the problem is still there. Do you have any idea why this difference between clients and servers? Do you know how can i fix it? Thanks. Duccio. AttachmentCemat path.pdf (87 Downloads) |
Follow us on