11/12/2019 1:48 PM | |
Joined: 3/13/2016 Last visit: 8/10/2022 Posts: 17 Rating: (0) |
Hello, I have a problem and i need to fix it as fast as a possible. Any ideas? Jakub Gawroński ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/12/2019 14:19:22New subject after splitting |
|
11/12/2019 2:15 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
Hello, i think you have the wrong HF5. there is a HF5 for Step7 V5.6 This HF5 need Step7 V5.6 without SP1 and there is a HF5 for Step7 V5.6 SP1 this is the one which you should install on you V5.6 SP1 Regards Christoph |
This contribution was helpful to1 thankful Users |
11/12/2019 2:36 PM | |
Joined: 3/13/2016 Last visit: 8/10/2022 Posts: 17 Rating: (0) |
Christoph, you are right, i was trying to install HF to Step without SP1. Thank you for your help! |
1/30/2020 1:52 PM | |
Posts: 1 Rating: (0) |
Many thanks also from me!
|
This contribution was helpful to1 thankful Users |
Follow us on