4/28/2021 2:16 PM | |
Posts: 198 Rating: (60) |
Hello, Which is the CFC version in use? Is this happening for specific charts or projects? Have you tried the same with any other project? From what is visible in the screenshot, it is the same window you would see if CFC was opened separately (from the Start Menu for instance) - ie., the selected chart is not triggered for opening. Have you tried these options: Right click on the respective chart in the plant hierarchy folder and select -> open object. Have you tried double clicking multiple times on the same chart? This could also be a product issue in which case it is advisable to consult the technical support for better advise on potential product upgrade if applicable. Hope this helps. |
Follow us on