5/2/2021 9:08 PM | |
Joined: 10/31/2019 Last visit: 8/9/2022 Posts: 3 Rating: (0) |
Pranav I attached parameters from the drive, which does not go into fault. You can see that P1300 is 0 and p1310 is 1310. I tried changing p1310 to 60, but it did not go to fault. The drive started running with no motor connected and did not go to fault.
It seems that I set Dynamic Drive control (DDC) to the drive which goes to fault as I would like. I will double check it tomorrow. Could it be that no-load monitoring does not work with standard drive control (SDC) and only works with DDC? Could I use DDC on small motors? Aux contacts are not an option, as I cannot add them at the moment. Regards Attachmentg120.pdf (209 Downloads) |
Follow us on