5/26/2021 3:02 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello Velmurugan Natarajan, see the FAQ in this regards with information and help. Why does the area length error warning appear in STEP 7 V5.5 with indirect addressing or when using FC100 "SWR_START"? I recommend also to use the command "Save as" together the option "With Reorganization (slow)" in the SIMATIC Manager. With best regards |
Follow us on