5/19/2021 12:47 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, The folder you describe is a Replica. It is a instance of a Model. A model is used when you have repeating functions like a tank. A model can contain the following elements: - CFC/SFC - OS pictures - OS reports - Additional documents If you create a model for a tank, you can create replica's of them (instances). The replica's are created using the Import Export Assistant. |
Last edited by: Oreca at: 05/19/2021 12:50:09If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on