5/29/2021 11:49 AM | |
Posts: 52 Rating: (1) |
Hello Team, I am using PCS7 V9.0 SP3 on VM. Following error i am getting after running WinCC for some time. "An error occur that requires a restart of computer. close all applications, if possible, and trigger a restart with ok buttons. Screen shot i have attached with post, some PC event logs also i have attached with this. Same problem Post i have seen on this forum, but solution given that post not resolve my problem. Is any one have face same and resolve this problem? then please share the how they resolve this. Thanks in Advance. Amol AttachmentImage (3).zip (156 Downloads) |
Last edited by: Amol Jadhav at: 05/29/2021 11:54:17Last edited by: Amol Jadhav at: 05/29/2021 11:55:21Last edited by: Amol Jadhav at: 05/29/2021 11:57:40 |
|
6/1/2021 9:15 AM | |
Posts: 198 Rating: (60) |
Hello Amol, Please provide more information for getting better solutions as the error in subject is quite general (there are multiple causes to this). To get started,
If yes, have you tried disabling redundancy and checking if you are still getting the same error after a subsequent OS download?
Also, please check these older forum posts which already addressed the same error under different scenarios: |
Last edited by: Jen_Moderator at: 06/01/2021 12:16:56Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on