6/23/2021 4:00 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello stewpid1, regarding to migration of STEP 7 V5.5 projects to TIA Portal see the FAQ and the point 11 of this FAQ in this case. You need all the optional package with the same version. Otherwise use the function "Save as" together with "With Reorganization (slow)" in STEP 7 V5.5. After repeat the migration in TIA Portal again. What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)? Cicero |
Follow us on